FFT Settings
FFT Points and Number Points are tightly coupled, so changes to one should be followed by changes to other.
Default Settings
Note: By Default, changing FFT Points will increase the # Points to Record proportionally for ease of use.
Effects of increasing FFT Points:
| Pros | Cons |
|---|---|
|
|
Effects of Increasing Number of Points
| Pros | Cons |
|---|---|
|
|
Examples will be shown in the Manual Tuning Section.
Review:
FFT Points and Number Points are tightly coupled, when one is modified, the other should be too.
To get better low frequency data, increase FFT Points to 32768, this will generate a frequency measurement at 0.25Hz. Also increase Number of Points to 240000 – if this is not increased, the measurement will likely be noisy.
Default settings are good for most systems. As loads get more complex, manual tweaking may be required to obtain a quality measurement.